The EOC Box is the next generation of overspeed controls for PowerShift Power Take Offs (PTOs). This option prevents vehicles from traveling on the road with their Power Take Off engaged. The New Chelsea EOC box is 75 percent smaller than the original version. The new circuitry will automatically senses if the vehicle has a 12 or 24 volt electrical system and adjusts accordingly. The EOC senses speed directly from the PTO drive gears instead of the alternator. This provides an accurate reading of RPM not subject to alternator problems or belt slippage. The unit is simple to set with easy to operate buttons. The LED lighting in the EOC has three settings for optimum operator visibility. The audio and visual blinking overspeed warning alerts the operator that the PTO is in the overspeed protection mode. The EOC Box in conjunction with a Chelsea PowerShift PTO offers superior protection to vehicles.
Markets:
• Aerial
• On-Highway
• Defense
• Construction
• Vocational & Municipal
Features/Benefits:
• PTO Auto kick-out to protect equipment
• Auto re-engage
• Compact design
Applications:
• Refuse
• Truck Cranes
• Pumper Cleaner
• Water Trucks